This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

secondary boot loader

Hi,

I'm compiling the mcu_plus_sdk_243x tcp server example.

I'm using  the AM243x EVB to load and run the program.

I see that the linker puts the main() in the DDR memory area.

Where is the code that initializes the DDR memory , before the program is loaded ?

Is it in the boot ?

I see that the boot makefile is auto generated.

How the boot parameters are set ?     -   Is it from the CCS properties ?

 Thanks,

Eli