Other Parts Discussed in Thread: MSPM0G3507
TI Friends & Family,
From our end customer ---
"Do we know if TI is doing any work to fix the lag in Theia between clicking the menu to build and the compiler running? It still stalls for several minutes in 1.1.0. The same is true for saving files; it takes several minutes before acting on the save request."
TI:
First off, this is great feedback for our teams, thanks for sharing and for your patience !
Secondly, I’d reply by saying simply “I haven’t seen this at this level of stalling” – but perhaps others have.
To clarify, Theia isn’t freezing or locking up when I click the save or rebuilt projects menu options. It’s just that nothing happens right away. It behaves as though it needs something to time out before servicing the request. Usually the request isn’t serviced for 3 – 5 minutes.
I would then ask if you are running on a machine that does this regularly (stalls on applications, builds, etc) and if you experience it only with the TI tools or not?
I only see this issue with Theia. I will note that the other 2 developers don’t experience this issue.
These are heavyweight tools (large installers, memory users, lots of interdependencies, etc). I just wonder if you witness stalls on other apps. Are you also saving locally or to a network drive or location? Is your machine for that matter all running locally or virtually/networked?
All other apps run without stalling. I save to my harddrive. All developer tools are run locally (not considering web based tools like Gitlab).
Outside of that, I don’t have much more to say. I run a high performance HP ZBook locally but do sometimes wish I had more RAM.
I’m running Windows 10 Enterprise
Intel(R) Core(TM) i7-10850H CPU @ 2.70GHz 2.71 GHz
32.0 GB RAM
Could you also share some insight on how the tool manages menu clicks so that I might find a way around this issue? For ex,
- Why does it take so long to decide to “Save All”? Does it actually only autosave at a fixed time interval?
- Is it right to see this number of processes running, and are there any specifically that can be closed when I want to click “Rebuild Project(s)”?
TI:
Regarding #1, we can’t seem to reproduce this either. This is the first time we are hearing of such an issue. Does it happen consistently with all projects? If so, can you try deleting the existing cache and start with a simple project in a new workspace and see if the issue persists?
Regarding #2, it is typical to have many CCS related processes in task manager.
It may be good to post this on E2E. Makes it easier to forward the issue to others and to have it tracked.
So...that's it! Posting for others to comment further please! BTW, this is for MSPM0G3507....
TY,
CY