Hi there,
I am having an issue with CCS (version 12.1.0.00007, though I don't think it is the version itself). I recently downloaded, installed, and set up CCS, and imported my project over. I tried to build it, but it cam back with 1 error reading
"This project was created using a version of compiler that is not currently installed - 4.4.8 [MSP430]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit CCS App Center to get the lastest compiler support. Or download and install the compiler, then register it with CSS through 'Preferences > CCS > Build > Compilers'."
I have followed the suggested routes listed above. Additionally, I have been through other forums with a similar issue but to no avail.
I believe that the issue lies with there being no connection to "">software-dl.ti.com/.../content.xml" since all the solutions I've seen seem to want to connect to this at some point. If this is the case, does anyone know when this will be back up? Or is there another work around I can use?