Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hello, I'm YPP In Byung Ho.
We are developing using TI CPU (RM48L952).
The system environment is as follows.
- a) CPU : RM48L952
- b) CCS : ver12.1.0.00007
- c) Compiler Version: TI v20.2.7.TLS
Our company is preparing for SIL (IEC61508) certification.
Therefore, the MISRA C (2012) standard is applied.
A warning message appears when applying the MISRA C standard.
Example)
1) MISRA_C_2012_11_04 Violation
- Conversion between volatile uint32 * pointer type and unsigned int type is performed.
- sys_selftest.c file.
- void errata_PBIST_4(void) Function.

2) MISRA_C_2012_11_08 Violation
- A conversion was performed to explicitly remove the volatile of the config INSTRUCTION_t
- A conversion was performed to explicitly remove the volatile from the volatile structure 1RamBase
- het.c
- void hetInit(void) Function

All violations must be handled by applying the MISRA C standard.
1) How to handle the above violation sources (process according to MISRA C standard)
2) The MISRA C rule is said to have been <APPROVED> in the above violation comment, but the evidence for exception handling
There are many violations as examples.
Please let me know how to handle the violation.
thanks