Other Parts Discussed in Thread: C2000WARE
Hello
I have imported the "clb_ex10_timer_two_states" project for test.
I am able to open the "clb_ex10_timer_two_states.syscfg" file and I have added in the Tile Design the option to generate the CLB simulation file.
When I run a build with diagram generation in the "Post-build steps". The build is OK and I can see the diagram files.
echo "========= Build of the CLB simulation has moved to the CLB Tool. Click the '?' icon by the _Generate CLB Simulation File_ enable for more details (located in
the Global Parameters of the Tile Design SysConfig module) ============="
${NODE_TOOL} "${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/dot_file_libraries/clbDotUtility.js" "${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/" "${BuildDirectory}/syscfg" "${BuildDirectory}/syscfg/clb.dot"
mkdir "${BuildDirectory}/diagrams"
${NODE_TOOL} "${C2000WARE_ROOT}/driverlib/.meta/generate_diagrams.js" "${C2000WARE_ROOT}" "${BuildDirectory}/diagrams" "${BuildDirectory}/syscfg"Now the problem:
In the CPU1_RAM/syscfg, when I open the clb_simulation.sh here is what I see:
mkdir "../simulation/" g++ -c -DCLB_SIM -I/usr/bin/systemc-2.3.3/src -I/home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc/include/type3 -I -Og -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MF../simulation/clb_sim.d -MT../simulation/clb_sim.o -I/syscfg -fno-threadsafe-statics -o../simulation/clb_sim.o ../syscfg/clb_sim.cpp g++ -DCLB_SIM -Og -g -gdwarf-3 -gstrict-dwarf -Wall -Wl,-Map,../simulation/simulation_output.map -L/usr/bin/systemc-2.3.3/build/src -o../simulation/simulation_output ../simulation/clb_sim.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_FSM_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_HLC_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_AOC_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_LUT4_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_OutputLUT_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_counter_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_counter_top_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_FSM_top_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_LUT4_top_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_OutputLUT_top_SC_model.o -Wl,--start-group -lsystemc -Wl,--end-group cd "../simulation/" "./simulation_output"
The path to system-c.2.3.3 is wrong (not in /usr/bin/). How can I change it automatically?
The path to systemc & system_linux are corrects.
When I run the file with correct path to system-c.2.3.3 on both lines, I have some errors and the vsd file is not generated.
The clb_simulation folder is not empty (clb_sim.d, clb_sim.o, simulation_output (4.8Mo), simulation_output.map)
/usr/bin/ld: BFD assertion (GNU Binutils for Ubuntu) 2.38 a échoué ../../bfd/reloc.c:8580 /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc-2.3.3/build/src/libsystemc.a(sc_clock.cpp.obj):sc_clock.cpp:(.pdata$_ZNK7sc_core9sc_object16get_child_eventsEv+0x0) : relocalisation dangereuse : collect2: fatal error: ld terminated with signal 11 [Erreur de segmentation], core dumped compilation terminated.
When I copy/paste the content of clb_simulation.sh in "Post-build steps" I have the same problem.
echo "========= Build the vsd file for simulation ========= "
mkdir "${BuildDirectory}/simulation/"
g++ -c -DCLB_SIM -I/home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc-2.3.3/src -I/home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc/include/type3 -I -Og -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MF${BuildDirectory}/simulation/clb_sim.d -MT${BuildDirectory}/simulation/clb_sim.o -I${BuildDirectory}/syscfg -fno-threadsafe-statics -o${BuildDirectory}/simulation/clb_sim.o ${BuildDirectory}/syscfg/clb_sim.cpp
#g++ -DCLB_SIM -Og -g -gdwarf-3 -gstrict-dwarf -Wall -Wl,-Map,${BuildDirectory}/simulation/simulation_output.map -L/home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc-2.3.3/build/src -o${BuildDirectory}/simulation/simulation_output ${BuildDirectory}/simulation/clb_sim.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_FSM_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_HLC_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_AOC_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_LUT4_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_OutputLUT_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_counter_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_counter_top_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_FSM_top_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_LUT4_top_SC_model.o /home/jerome/ti/c2000/C2000Ware_5_00_00_00/utilities/clb_tool/clb_syscfg/systemc_linux/src/type3/CLB_OutputLUT_top_SC_model.o -Wl,--start-group -lsystemc -Wl,--end-group
cd "${BuildDirectory}/simulation/"
chmod +x "simulation_output"
"./simulation_output"
Do you have any advice to help me?
My configuration is :
Ubuntu 22.04
CCS 12.4.0.00007
C2000Ware 5.00.00.00
ti-cgt-c2000_22.6.0LTS
Thanks you for your help.
Jérôme