The following occurred today while checking for updates in ccsv5.1 M6.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mike,
This is a known item as v5.1 is still pre-release.
I actually would not suggest doing an update at this point as if you remove those sites from the list, the one update that will be found will actually be a little problematic with CCS.
However if you wish to try it, some options you are are the following
1) If you wish to check for updates. For the time being you can go to Window->Preferences->Install/Update. If you expand this tab you will see "Available Software Sites" and this is where you can configure the list of sites searched when scanning for updates and features. If you remove the sites listed above that are not being found you should be able to run the update.
2) If there is a specific extension/update/feature you need or wish to install, then you can go to Help -> Install New Software and use that option.
I hope this helps and our appologies for the inconvenience.
Best Regards,
Lisa