Hi-
I need some help building a project that was imported as a legacy CCSv3 project. The project has a main directory and below that a TI directory with support directories and files in it. The main directory .c files build fine, but some of the files in the TI directory don't build because the include file path won't allow the compiler to find the included .h files. I've been looking at the 'make' files and the include paths for that directory are wrong. How do I fix the include path for the TI directory? They are fine for the main project directory.
Thanks in advance-
Mary at Agilent