Hi,
I would like to ask a question on target connection.
In CCS 3.3 one can use shortcut ALT+C to connect/disconnect, which is very convenient. In CCS 4’s help I found the following information:
However, it seems that there is no such “connect button” in my CCS 4, at least not in the default layout. I also searched different menus including View, Project, Target, Tools and cannot found option to get this “connect button” displayed.
Does it really exist in 4? How can I enable it?
Update:
I have found connect(ALT+C)/disconnect(ALT+D) are available in Debugging mode. However, there is a difference with 3.3 is that Disconnect doesn’t actually remove the connection with the target, and can be instantly re-connected with ALT+C. It appears to me that both Connect/Disconnect doesn’t do actual hardware JTAG connection/disconnection, unlike in 3.3.
Also in 3.3, every Connect following Disconnect reloads the GEL file, but there is no corresponding behavior here at all.
So what is the really going on with Connect/Disconnect here, and why is it designed to be different from behavior in 3.3?
Zheng