Other Parts Discussed in Thread: TMS320C6472
Hi,
just a quick question and a comment on the register display.
running CCS 4.2.0.10012 on the Einfochips TMDSEVM6472.
I noticed that there is no selection for the tsip(0,1,2) registers - that i could find.
Also the PPL(0,1,2)GEM register definitions seem to be incorrect for the C6742 flavor per (SPRS612F). Some of the fields ( like ALNCTL ) should not be defined for the C6472 case and other important ones are missing. Is there any method to change what registers are displayed for a particular processor ( through some configuration or menu ) that i have not come across?
From other threads on this forum , i understand that the ..targetdb\Modules\c6472\cslr_pllc.xml is probably the issue. I did not want to hack it up - if a newer version is available.
Thanks