This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Handling SVN branch in CCSv4

I have a CCSv4 workspace with a single project. The project source files exist on a remote file server under SVN control. We have branched the source to a new version, so I wish to change CCS so I can develop within the new source branch. What is the best way to accomplish this? I figured that I should copy the current workspace (say, WSpace_v1.0) and rename it to WSpace_v2.0. Works fine except that I cannot figure out how to change the location of the source files. The old CCSv3 .pjt files were text-based and could be changed with the Find/Replace tool in any editor. I suppose it isn't so, but It would be nice if this were the case with CCSv4. Any help will be appreciated.

Thanks,

Steve