I would like to run Code Composer Studio on an ARM system, specifically the RaspberryPi 4. I have a target device I need to reach that is attached to a USB-to-serial connection on a raspberrypi machine.
Since CCS 12.x is compiled for Linux, all that would be required is change from x86 compilation to cross-compile to the Cortex-A72 chipset that the Linux Debian-based operating system is running. This should only be a small change to the makefile(?) which builds CCS today! (example : CFLAGS = -Wall -mfpu=neon-vfpv4 -mcpu=cortex-a7 )
Can this be compiled and made available ?
Reference installation attempt, notice the system arch is aarch64.
pi@remora:~/download/CCS12.5.0.00007_linux-x64$ ./ccs_setup_12.5.0.00007.run
-bash: ./ccs_setup_12.5.0.00007.run: cannot execute binary file: Exec format error
pi@remora:~/download/CCS12.5.0.00007_linux-x64$ file ccs_setup_12.5.0.00007.run
ccs_setup_12.5.0.00007.run: ELF 64-bit LSB executable, x86-64, version 1 (SYSV), dynamically linked, interpreter /lib64/ld-linux-x86-64.so.2, for GNU/Linux 2.4.0, stripped
pi@remora:~/download/CCS12.5.0.00007_linux-x64$ uname -a
Linux remora 6.1.21-v8+ #1642 SMP PREEMPT Mon Apr 3 17:24:16 BST 2023 aarch64 GNU/Linux
pi@remora:~/download/CCS12.5.0.00007_linux-x64$ cat /etc/*rel*
PRETTY_NAME="Debian GNU/Linux 11 (bullseye)"
NAME="Debian GNU/Linux"
VERSION_ID="11"
VERSION="11 (bullseye)"
VERSION_CODENAME=bullseye
ID=debian
HOME_URL="">https://www.debian.org/"
SUPPORT_URL="">www.debian.org/support"