Part Number: CODECOMPOSER
Hi
This bug has been here for quite some time, And I finally got around to report it ;-)
If I edit a ccxml target config file using the GUI, each time i save it adds a newline to each line.
While it does not break any functionality in CCS, it is quite annoying as it ads a lot of noise to the version control, in these two cases:
- During development I temporarily changed a setting. I.e. experimented with the TCLK Frequency, but returned to same setting.
- Now the version control, claims I did a change to the ccxml file, but upon closer inspection, it is only those extra newlines.
- I do make a change, and keep that change.
- Now the merge in version control is getting harder as I not see the actual change but also all the redundant extra newlines. Telling the diff tool to ignore white space takes away some noise but not all.
It has a strong smell of a bug in the handling of different line ending types (Dos/Unix).
To illustrate I made a few screenshots with the font set to ridiculous small, to get the broader picture in a screenshot.
Screenshot of noisy diff

The same diff except here i manually removed the redundant newlines.

CCS version (I have seen this in many older versions too)
Code Composer Studio
Version: 12.5.0.00007OS: Windows 10, v.10.0, x86_64 / win32
Java vendor: Eclipse Adoptium
Java runtime version: 11.0.13+8
Java version: 11.0.13