Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310,
Hi,
I have a problem loading a program to my LAUNCHXL-CC1310, the point is the memory is not enough big and gives me the following error: "program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment fails for section ".cinit" size 0x306. Available memory ranges: CC1310_LAUNCHXL_TIRTOS.cmd".
The proyect I've used is a custom from a sample downloaded in resoruce explorer (rfEchoTx_CC1310_LAUNCHXL_tirtos_ccs) and I think the error message has come cause the proccesor specified in proyect properties is CC1310F32 and it should be 128 which is the one it is used in the board. I try to import the same proyect cause it has CC1310F128 by default and I can build and load the program into my board but it does not work at all cause the radio signal seems not being received by the board I'm using as Rx.
I appreciate any suggest to make my programe works.