http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/126114.aspx
Both of these documents similarly describe the issue that I am experiencing.
With each, the ‘solution’ is the same.. update the SWT Library used by eclipse, this problem will be solved in version 4.2.2
We are running Version: 4.2.3.00004
I have updated the SWT Library as suggested.
Org.eclipse.swt Version 3.4.0.v3448f
Org.eclipse.swt.win32.win32.x86 3.4.0.v3448f
Attached image shows a missing dropdown. The Environment tab and Macros tab are both blank.
Furthermore, from the shortcut for Code Composer, I have set the Privelege Level to Run as Administrator, Disabling visual themes, disable desktop composition and disable display scaling on high DPI settings. Using these settings, I am able to see what is on the attached image. When these settings are default, I am able to see nothing on the build steps tab.