Other Parts Discussed in Thread: TMS320VC5505
I'm using the CCS V4.2.4.00033. After loading the program, I find that CCS can't open the memory window. If I do it, CCS will give a error. error is "C55xx: Trouble Reading Memory Block at 0x1 on Page 2 of Length 0x7e: (Error -1069 @ 0xFC) Device memory bus has an error and may be hung. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Release 5.0.429.0) ".
Anybody knows the reasons?