This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with TMS320C6416 DSK.

Other Parts Discussed in Thread: TMS320C6416

I have a TMS320C6416 DSK,i'm using Windows 7, CCS v3.1 on CD is not running in Windows 7. I setup CCS V4, running OK, but when i connect board to PC with USB and run debug. A message on Console dialog is: "Invalid file format". I can't fix it, please help me!

  • Hello,

    It sounds like you are doing a 'Debug Active Project' and the project setting are incorrect for the target, hence the built executable cannot be loaded. Double check your project setting and make sure they look correct.

    Thanks

    ki