Hi
When I try to start the vendor demon tidspssw I get the folowing error
(tidspssw) Vendor daemon can't talk to lmgrd (Cannot connect to license server system. (-15,570:115 "Operation now in progress"))
I am using lmadmin
the conssole.log is as folows
14:54:04 (tidspssw) FLEXnet Licensing version v11.4.100.0 build 50818 i86_re3
14:54:04 (tidspssw) lmgrd version 11.10, tidspssw version 11.4
14:54:04 (tidspssw) lmremove disabled
The server is a Debian 64 bit system
Dose any one have any clues?