This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

License & installation question

Is there any way to tell if you originally installed the micro-controller or the platinum edition? We are having a license audit done internally, and they say my license is for the micro-controller version, but I think I selected the platinum version when I originally did the install using the 30-day free license. Then when the licenses finally got installed on our server by IT, I re-configured to use the licenses from the server. Do I need to do an un-install and re-install to be sure I have the micro-controller version installed, or is there some way to tell which version I currently have installed?