This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Save Memory option in Version: 5.0.1.201105110900

Where is the Save Memory option for CCSv5.0.1 ?? In the Memory browser I am able to Copy to Clipboard only the values which i can select but there is no option to save the memory of a particular length from a specific address to a file. This option was there in CCSv4. Is this option removed in CCSv5.0.1??

  • Hi,

    I can find this option in CCSv5.0.2 by right-clicking on the memory browser (check the attached screen).

    If you can't find this option, I strongly suggest you updating your version of CCS, as several bugs and features have been implemented since 5.0.1 was launched. In order to not disrupt your work, you can install the new version in a different directory and open a new workspace (they coexist very well this way).

    Hope this helps,

    Rafael

  • Hi,

    I have a problem with the save memory, too. I want to read out the flash memory at 0x14000.

    If I make the configuration like in the picture I get data from address 0x4000 back (see notepad file).

     

     

    thanks,

    Georg