Hi all ,
I am using matlab 2009b and ccs V3.3 platinum version . i made a smal project in Simulink for TMS32DM6437 processor.
But when press in button "Incremental Build" to generate the code for CCS, appear a error dialog window with next
message:
==================================================
The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error:
Error while instantiating CCSLinkTgtPkg.Board class.
Caused by:
Could not obtain board configuration from Code Composer Studio(TM). Make sure that Code Composer Studio and Embedded IDE Link are installed and properly registered.
Caused by:
Error map is empty.
The build process will terminate as a result.
====================================================================.
Is matlab 2009b compatibility with ccs v3.3 .
What is this error and what would be the solution for this .