Hi
I'm a new user of CCS4. I'm trying to follow the demo code: FBPS.pjt (provided in sprc711.zip). This demo program and user guide are based on CCS3 which may cause some difference in CCS4. Could anyone help me a little on below points? Thanks a lot in advance.
1. CCS4 watch window doesn't work
when I'm running the code, the watch window throws some error messages as below:
he message shows: couldn't read memory at 0x0000AAC0@data Execution state prevented access.
Why it has such errors? Did I use a wrong setup somewhere?
2. In the PBPS user guide, it mentions DEBUG-Real-time Mode many times. But it seems I didn't find that in CCS4. In CCS4, after rebuiling the project, I click "launch TI debugger", then I "load program", then I click "Run". Is this the corresponding real-time mode in CCS4?
Thank you very much,
Violet