Hi !
I running CCS 4.2.4.00033 on a VMware Player 3.1.4 running Win XP SP3.
I have a floating licence.
If I try to use CCS on a host PC running Win XP SP3, I have no problem, I have "Code Composer Studio (Licensed) on the top of the CCS windows in all cases.
On CCS running on the VMware Player, I have "Code Composer Studio (Licensed : X days Remaining).
I can see in the file "licenselocation.txt" that the license server address and port are OK.