Other Parts Discussed in Thread: SYSCONFIG
Our project builds fine in CCS12.4. The same project opened in 12.5 is not buildable due some device selection problem:
**** Build Finished **** Buildfile generation error occurred.. This project was created for a device not currently recognized - Cortex R.AM263x.AM263x_CC: - Re-run CCS installer on your existing CCS location, ensure the Product Family for your device is selected, and proceed with installation if it wasn't. - See 'Help > Check for Updates' to check if support for this device is available through a CCS update. - Migrate the project to closest matching supported device by adjusting project properties. - Or contact TI for support if using experimental silicon. Build stopped..
Note the advice given is not relevant since I can build example project for AM263x just fine.
I tried to rectify the problem in the SysConfig section but it shuts me out.

It looks like the .syscfg file needs some hand edits before CCS12.5 will accept it.
Thank you.