Hello,
I'm using K2K EVM in which external XDS2xx MIPI is connected for JTAG Interface.
I'm facing issue to establish the target. It shows below error-
C66xx_0: Error connecting to the target: (Error -1180 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.4.0.00006)
After removing the device from reset, its shows error as below -
C66xx_0: Error connecting to the target: (Error -6306) Failed to connect to PRSC module. (Emulation package 8.4.0.00006)
I checked voltages, it is proper. Can you pls suggest any solution to this issue.

Thanks,
Chaithra Kulal