Part Number: LAUNCHXL-CC26X2R1
Hi Team,
I am trying to modify several GPIO interfaces of the CC2642 to SPI interfaces to drive my SPI device (RC522 card reader). The SPI interface names and pin definitions I want to use are as follows:
// SPI Pin Definitions
#define NFC_SPI_MISO IOID_14 // MISO pin for NFC SPI
#define NFC_SPI_MOSI IOID_15 // MOSI pin for NFC SPI
#define NFC_SPI_CLK IOID_25 // Clock pin for NFC SPI
#define NFC_SPI_CS IOID_26 // Chip select pin for NFC SPI
My development board is CC26X2R1_LAUNCHXL, and the compilation environment is CCS10.1.1. I have rewritten an SPI driver, including two files, board_spi.c and board_spi.h (see attachment), and also added an SPI interface defined according to my pin definition in .syscfg. However, after downloading it to the development board, I am unable to perform SPI communication with other devices from the pins I defined. I have tried many methods, but it seems that this self-defined SPI interface can never be opened. I would like to ask if there is a problem with my driver. Or is there some other setting I did wrong? Thank you for your help.
/*********************************************************************
* INCLUDES
*/
#include "board_spi.h"
/********************* Macro Definitions ************************/
// Enumeration for SPI instances on CC2642R1
typedef enum CC2642R1_SPIName {
CC2642R1_SPI0 = 0,
CC2642R1_SPICOUNT
} CC2642R1_SPIName;
// SPI objects for CC2642R1
SPICC26X2DMA_Object NFC_spiCC26X2DMAObjects[CC2642R1_SPICOUNT];
/********************* Internal Variables ************************/
// Hardware attributes for SPI on CC2642R1
const SPICC26X2DMA_HWAttrs NFC_spiCC26X2DMAHWAttrs[CC2642R1_SPICOUNT] = {
{
.baseAddr = SSI0_BASE, // Base address for SPI
.intNum = INT_SSI0_COMB, // Interrupt number
.intPriority = ~0, // Interrupt priority
.swiPriority = 0, // Software interrupt priority
.powerMngrId = PowerCC26XX_PERIPH_SSI0, // Power manager ID
.defaultTxBufValue = 0, // Default value for transmit buffer
.rxChannelBitMask = 1<<UDMA_CHAN_SSI0_RX, // Bit mask for RX channel
.txChannelBitMask = 1<<UDMA_CHAN_SSI0_TX, // Bit mask for TX channel
.mosiPin = NFC_SPI_MOSI, // MOSI pin configuration
.misoPin = NFC_SPI_MISO, // MISO pin configuration
.clkPin = NFC_SPI_CLK, // Clock pin configuration
.csnPin = NFC_SPI_CS // Chip select pin configuration
}
};
// SPI configuration for CC2642R1
const SPI_Config SPI0_config[CC2642R1_SPICOUNT] = {
{
.fxnTablePtr = &SPICC26X2DMA_fxnTable, // Pointer to function table
.object = &NFC_spiCC26X2DMAObjects[CC2642R1_SPI0], // Pointer to SPI object
.hwAttrs = &NFC_spiCC26X2DMAHWAttrs[CC2642R1_SPI0] // Pointer to hardware attributes
},
};
// Count of SPI instances
const uint_least8_t SPI0_count = CC2642R1_SPICOUNT;
// SPI interface
//static PIN_Handle NFC_hspiPin = NULL; // Deprecated: Handle for SPI pin (not used)
static SPI_Handle NFC_spiHandle = NULL; // Handle for SPI
static SPI_Params NFC_spiParams; // Parameters for SPI
/********************* Internal Function Declarations ************************/
// Declaration for internal function to open SPI0
static bool NFC_SPI0_Open(NFC_U32 NFC_bitRate);
//**********************************************************************
// Name: NFC_SPI0_Open
// Description: Opens the SPI interface
// Parameters: NFC_bitRate - Desired SPI speed
// Return: True if operation is successful, false otherwise
// Author: 甜甜的大香瓜
// Email: [email]
// QQ group: 香瓜BLE之CC2640R2F(557278427)
// Shop: opengua.taobao.com
// Change time: 2021.08.02
//**********************************************************************
bool NFC_SPI0_Open(NFC_U32 NFC_bitRate)
{
/* Configure SPI as master */
SPI_Params_init(&NFC_spiParams);
NFC_spiParams.frameFormat = SPI_POL0_PHA1; // Frame format configuration
NFC_spiParams.bitRate = NFC_bitRate; // Set SPI speed
NFC_spiParams.mode = SPI_MASTER; // Set SPI mode as master
NFC_spiParams.transferMode = SPI_MODE_BLOCKING; // Set transfer mode
/* Attempt to open SPI. */
NFC_spiHandle = SPI_open(CC2642R1_SPI0, &NFC_spiParams);
return NFC_spiHandle != NULL;
}
/*********************************************************************
* LOCAL VARIABLES
*/
// SPI handle and parameters
//static SPI_Handle s_spiHandle; // Deprecated: SPI handle (not used)
//static SPI_Params s_spiParams; // Deprecated: SPI parameters (not used)
static SPI_Transaction s_spiTransaction; // SPI transaction structure
// SPI chip select pin
static PIN_State s_spiCsnState; // State for chip select pin
static PIN_Handle s_spiCsnHandle; // Handle for chip select pin
static PIN_Config s_spiCsnPinsCfg[] = // Configuration for chip select pins
{
NFC_SPI_CS | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MIN,
PIN_TERMINATE
};
/*********************************************************************
* PUBLIC FUNCTIONS
*/
/**
@brief Initialization function for SPI
@param None
@return None
*/
bool SPI_Init(void)
{
bool nNFC_f;
// Initialization of SPI chip select handle
s_spiCsnHandle = PIN_open(&s_spiCsnState, s_spiCsnPinsCfg);
// Initialize SPI module
SPI_init();
// Open SPI0 with specified bit rate
nNFC_f = NFC_SPI0_Open(NFC_SPI0_RATE);
return nNFC_f;
}
/**
@brief Sets the SPI chip select signal
@param pinId -[in] Pin number
@param pinState -[in] Pin state
@return None
*/
void SPI_CsnSet(PIN_Id pinId, bool pinState)
{
if(pinState == NFC_SPI_CS_OFF)
{
PIN_setOutputValue(s_spiCsnHandle, pinId, 1); // Set pin high
}
else if(pinState == NFC_SPI_CS_ON)
{
PIN_setOutputValue(s_spiCsnHandle, pinId, 0); // Set pin low
}
}
/**
@brief Performs SPI read/write operation
@param pWriteData -[in] Data to write
@param pReadData -[out] Data read
@param writeDataLen -[in] Length of data to write
@return None
*/
void SPI_ReadWriteData(uint8_t *pWriteData, uint8_t *pReadData, uint8_t writeDataLen)
{
bool transferOk;
s_spiTransaction.count = writeDataLen; // Length of data to write
s_spiTransaction.arg = NULL;
s_spiTransaction.txBuf = pWriteData; // Transmit buffer
s_spiTransaction.rxBuf = pReadData; // Receive buffer
// Start SPI transfer
transferOk = SPI_transfer(NFC_spiHandle, &s_spiTransaction);
if(!transferOk)
{
// Handle error in SPI transfer or if transfer already in progress.
}
}
/*************************************END OF FILE*************************************/