Hi,
There's a switch somewhere in CCS12 that allows the display of special characters for the common C type operators such as !=, <= and >= etc. I had this active previously since I noticed them being displayed in the source code, but something got tweaked somewhere (maybe it was me) and now they are displayed as default operators, and I can't find the option to have them displayed as special operators ...
Where is the switch in the CCS12 options to display these standard comparison operators as special characters ≤ , ≥ and ≠ please ??
Cheers, MM