Hello,
I am using CCS v5.0.3.00028 and have noticed that selecting variables within my code (either single clicking or double clicking) generates many error events within the Error Log view. Below is an example of such an error. My CCS installation is clean in that no other versions of CCS was on the machine before I installed this version. I also downloaded and installed the BIOS-MCSDK (http://software-dl.ti.com/sdoemb/sdoemb_public_sw/bios_mcsdk/latest/index_FDS.html). It seems like there is something wrong in my installation but I am not sure.
----------------------------------------
eclipse.buildId=M20100909-0800
java.version=1.5.0_14
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Command-line arguments: -os win32 -ws win32 -arch x86
Error
Fri Aug 26 10:21:29 CDT 2011
Error
java.nio.channels.ClosedByInterruptException
at java.nio.channels.spi.AbstractInterruptibleChannel.end(Unknown Source)
at sun.nio.ch.FileChannelImpl.size(Unknown Source)
at org.eclipse.cdt.internal.core.parser.scanner.FileCharArray.create(FileCharArray.java:44)
at org.eclipse.cdt.internal.core.parser.InternalParserUtil.createFileContent(InternalParserUtil.java:201)
at org.eclipse.cdt.internal.core.parser.InternalParserUtil.createExternalFileContent(InternalParserUtil.java:188)
at org.eclipse.cdt.core.parser.FileContent.createForExternalFileLocation(FileContent.java:90)
at org.eclipse.cdt.internal.core.parser.SavedFilesProvider.getContentForInclusion(SavedFilesProvider.java:41)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor$1.checkFile(CPreprocessor.java:103)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor$1.checkFile(CPreprocessor.java:1)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor.findInclusion(CPreprocessor.java:966)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor.executeInclude(CPreprocessor.java:1251)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor.executeDirective(CPreprocessor.java:1067)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor.internalFetchToken(CPreprocessor.java:726)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor.fetchToken(CPreprocessor.java:469)
at org.eclipse.cdt.internal.core.parser.scanner.CPreprocessor.nextToken(CPreprocessor.java:563)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.fetchToken(AbstractGNUSourceCodeParser.java:260)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.nextToken(AbstractGNUSourceCodeParser.java:284)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.acceptInactiveCodeBoundary(AbstractGNUSourceCodeParser.java:345)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.declarationList(AbstractGNUSourceCodeParser.java:1283)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.parseTranslationUnit(AbstractGNUSourceCodeParser.java:1253)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.translationUnit(AbstractGNUSourceCodeParser.java:1248)
at org.eclipse.cdt.internal.core.dom.parser.AbstractGNUSourceCodeParser.parse(AbstractGNUSourceCodeParser.java:645)
at org.eclipse.cdt.core.dom.parser.AbstractCLikeLanguage.getASTTranslationUnit(AbstractCLikeLanguage.java:143)
at org.eclipse.cdt.internal.core.model.TranslationUnit.getAST(TranslationUnit.java:806)
at org.eclipse.cdt.internal.core.model.TranslationUnit.getAST(TranslationUnit.java:766)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.rtsc.xdctools.ui.contentassist.RTSCHelpProvider.getFunctionSummaries(RTSCHelpProvider.java:69)
at org.eclipse.rtsc.xdctools.ui.contentassist.RTSCHelpProvider.getFunctionInfo(RTSCHelpProvider.java:146)
at org.eclipse.rtsc.xdctools.ui.contentassist.RTSCHelpProvider.getFunctionInfo(RTSCHelpProvider.java:1)
at org.eclipse.cdt.internal.ui.text.CHelpSettings.getFunctionInfo(CHelpSettings.java:121)
at org.eclipse.cdt.internal.ui.CHelpProviderManager.getFunctionInfo(CHelpProviderManager.java:163)
at org.eclipse.cdt.internal.ui.text.c.hover.CDocHover.getHoverInfo(CDocHover.java:84)
at org.eclipse.cdt.internal.ui.text.c.hover.AbstractCEditorTextHover.getHoverInfo2(AbstractCEditorTextHover.java:83)
at org.eclipse.cdt.internal.ui.text.c.hover.BestMatchHover.getHoverInfo2(BestMatchHover.java:149)
at org.eclipse.cdt.internal.ui.text.c.hover.CEditorTextHoverProxy.getHoverInfo2(CEditorTextHoverProxy.java:86)
at org.eclipse.jface.text.TextViewerHoverManager$4.run(TextViewerHoverManager.java:166)