This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem in building project from simulink

i can't run a model in simulink on DM6437 with ccs 3.1

### Connecting to Code Composer Studio(tm) ...
### Generating code into build directory: C:\Users\Engineer\Documents\MATLAB\testdm_ccslink
### Invoking Target Language Compiler on testdm.rtw
 tlc
 -r
 C:\Users\Engineer\Documents\MATLAB\testdm_ccslink\testdm.rtw
 C:\Program Files\MATLAB\R2009a\toolbox\rtw\targets\ccslink\ccslink\ccslink_grt.tlc
 -OC:\Users\Engineer\Documents\MATLAB\testdm_ccslink
 -IC:\Program Files\MATLAB\R2009a\toolbox\rtw\targets\ccslink\ccslink
 -IC:\Program Files\MATLAB\R2009a\toolbox\rtw\targets\tic6000\tic6000blks
 -IC:\Users\Engineer\Documents\MATLAB\testdm_ccslink\tlc
 -IC:\Program Files\MATLAB\R2009a\rtw\c\tlc\mw
 -IC:\Program Files\MATLAB\R2009a\rtw\c\tlc\lib
 -IC:\Program Files\MATLAB\R2009a\rtw\c\tlc\blocks
 -IC:\Program Files\MATLAB\R2009a\rtw\c\tlc\fixpt
 -IC:\Program Files\MATLAB\R2009a\stateflow\c\tlc
 -aEnforceIntegerDowncast=1
 -aFoldNonRolledExpr=1
 -aInlineInvariantSignals=0
 -aInlineParameters=0
 -aLocalBlockOutputs=1
 -aRollThreshold=5
 -aZeroInternalMemoryAtStartup=1
 -aZeroExternalMemoryAtStartup=1
 -aInitFltsAndDblsToZero=0
 -aForceBlockIOInitOptimize=0
 -aGenerateReport=0
 -aGenCodeOnly=1
 -aRTWVerbose=1
 -aIncludeHyperlinkInReport=0
 -aLaunchReport=0
 -aGenerateTraceInfo=0
 -aForceParamTrailComments=0
 -aGenerateComments=1
 -aIgnoreCustomStorageClasses=1
 -aIncHierarchyInIds=0
 -aMaxRTWIdLen=31
 -aShowEliminatedStatements=0
 -aIncDataTypeInIds=0
 -aInsertBlockDesc=0
 -aIgnoreTestpoints=0
 -aSimulinkBlockComments=1
 -aInlinedPrmAccess="Literals"
 -aTargetFcnLib="ansi_tfl_table_tmw.mat"
 -aIsPILTarget=0
 -aLogVarNameModifier="rt_"
 -aGenerateFullHeader=1
 -aexportIDEObj=1
 -aideObjName="CCS_Obj"
 -aProfileGenCode=0
 -aInlineDSPBlks=1
 -abuildAction="Build_and_execute"
 -acompilerOptionsStr=""
 -alinkerOptionsStr=""
 -asystemStackSize=8129
 -aoverrunNotificationMethod="None"
 -aoverrunNotificationFcn="myfunction"
 -aGenerateASAP2=0
 -aGenerateTraceInfo=0
 -aIgnoreTestpoints=0
 -aProfileNumSamples=100
 -aideObjBuildTimeout=1000
 -aideObjTimeout=10
 -aoldideObjBuildTimeout=1000
 -aoldideObjTimeout=10
 -asystemStackSize=8129
 -p10000


### Loading TLC function libraries

.....
### Initial pass through model to cache user defined code
### Caching model source code
.....................
### Writing header file testdm_types.h
### Writing header file testdm.h
.
### Writing source file testdm.c
### Writing header file testdm_private.h
### Writing header file rtmodel.h
### Writing source file testdm_data.c
.
### Writing header file rt_nonfinite.h
### Writing source file rt_nonfinite.c
### Writing header file rtGetInf.h
### Writing source file rtGetInf.c
.
### Writing header file rtGetNaN.h
### Writing source file rtGetNaN.c
### Writing source file testdm_main.c
### Writing header file testdm_main.h
.
### Writing header file MW_c6xxx_csl.h
### Writing source file MW_c6xxx_csl.c
### TLC code generation complete.
### Creating project: C:\Users\Engineer\Documents\MATLAB\testdm_ccslink\testdm.pjt
### Project creation done.
### Building project...  <------  this place has a error

error:

Error building Real-Time Workshop target for block diagram 'testdm'. MATLAB error message: The call to ccslink_grt_make_rtw_hook, during the exit hook generated the following error: Error while building the project. Caused by: Build complete: 3 errors, 0 warnings. The build process will terminate as a result.

help me please