This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Project Level Predefined Symbols For Multiple Build Configurations

Hello,

I have two build configurations. 90% of the predefined symbols are the same in both.

To avoid having to remember to insert a new predefined symbol into two build configurations, I'd like to define it once for the whole project.

Is there some way to define predefined symbols at the project level such that they are applicable for all build configurations please?

Thank you.