The minimum system requirement for installing XDS560v2: Code Composer Studio™V5.0
Note: Linux Operating System only supports Linux Version CCSv5.0 and its above versions. Before installing the driver, please make sure that the Linux version CCSv5.0 has been installed.
There are various kinds of Linux versions, about the Linux version which CCS5.x supports and the chips that the CCS supports, please refer to: http://processors.wiki.ti.com/index.php/Linux_Host_Support
Take SEED-XDS560v2 as an example to introduce the detailed step of using XDS560v2 system trace jtag emulator to debug chip DM6446. Readers can download the document from "download center" of SEED official website: www.seeddsp.com/eng