This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 12.6 failed to install



Hi,

I cannot install latest versions of CCS - 12.5 and 12.6

Installation on Windows 10 Pro

McAfee Endpoint Security in place (cannot be switched off)

Offline installer is used.  (Web installer cannot be used - failed to obtain any packet)

Installation attempted also as an administrator.

Java support by Liberica JDK 17.x or 21.x (both tried)

java --version
openjdk 21.0.1 2023-10-17 LTS
OpenJDK Runtime Environment (build 21.0.1+12-LTS)
OpenJDK 64-Bit Server VM (build 21.0.1+12-LTS, mixed mode, sharing)

The problematic package is com.ti.emulation.pack.win64_12.6.0.00029.jar

Log (ti_emupack_12.6.0.00029_install.log):

Log started 01/18/2024 at 20:31:46
Preferred installation mode : unattended
Trying to init installer in mode unattended
Mode unattended successfully initialized
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] 
[20:31:46] Beginning Installation of MSVC Redistributable Packages
Preparing to Install
Preparing to Install
Directory already exists: C:\ti\ccs12.6.0\ccs\ccs_base\common\bin
Unpacking files
Unpacking C:\ti\ccs12.6.0\ccs\ccs_base\common\bin\ti_targetdb_parser.dll
Unpacking C:\ti\ccs12.6.0\ccs\ccs_base\common\bin\libusb.zip
Unpacking C:\ti\ccs12.6.0\ccs\ccs_base\common\bin\libusb-1.0.dll
Error copying file from packed archive C:/Users/<username>/AppData/Local/Temp/CCS_42~1/EMU_TI/TI_EMU~1.EXE to C:/ti/ccs12.6.0/ccs/ccs_base/common/bin/libusb-1.0.dll
There has been an error.
Unable to copy file
Exiting with code 1

This pack caused installation problems with previous releases (up to 12.4) also but those were resolved by installing the above mentioned Java support.

However with 12.5 and 12.6 this packet fails the whole installation. You cannot ignore this error so the installation finishes excluding the mentioned pack..

How this can be resolved?

  • Hello,

    McAfee Endpoint Security in place (cannot be switched off)

    Unfortunately, McAfee (along with Kaspersky) has historically given us the most trouble in regards to CCS installation. If you can't even temporarily disable it, can you at least whitelist the CCS installer and everything related to it? 

    What device are you planning on using with CCS?

    Thanks

    ki 

  • Hi,

    Thank you for the reply.

    Unfortunately I do not have a control over McAfee except "Update" and start "Scan". Configuration is protected by system administrators.

    But also there are no reported blocked or quarantined items.

    We are using CC2662R1 for wBMS platform.

    CCS 12.5 and 12.6 comes with a new compiler in place.

    Thank you

  • Please start a private E2E conversation with me to discuss your options.

    Thanks

    ki

  • Thank you.

    What helped me for this version of CCS (12.6) and CCS_theia (1.3):

    Update MSVC packages to the latest updates.

    Run the installer "As Administrator"

    If stops with Warning message -> hit "Retry"

    Note:

    Both installers fail with ti_emupack package. This needs to be investigated. If "Retry" step does not help, one could not install CCS at all!