I have a working project that was built using CCS 4.2.3. I had to upgrade to 4.2.4 to gain support for the new FRAM based MSP430. When I try to import the 4.2.3 project into 4.2.4 by either "Project -> Import Exisiting CCS Project" or "Project -> Import Legacy CCS Project" and browse to the source directory that contains the dot files and the .ccxml file, the tool does not recognize any of these as project files.
Anyone have an idea what could be wrong? Did the project file structure change between 4.2.3 and 4.2.4?