Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: SYSCONFIG
Is there a way to add conditional statements in syscfg file?
Something like:
#if defined DEBUG
XYZ.addr = 0x1000
#else
XYZ.addr = 0x5000
#endif
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: SYSCONFIG
Is there a way to add conditional statements in syscfg file?
Something like:
#if defined DEBUG
XYZ.addr = 0x1000
#else
XYZ.addr = 0x5000
#endif
Hi Manoj,
It is possible to add conditional statements when modifying SysConfig files inside of a text editor. Here is an openthread example and my own rudimentary example:
if(0) gpio.$name = "CONFIG_GPIO_LED_0"; else gpio.$name = "CONFIG_GPIO_LED_HI";
Where simply changing 0 to 1 causes the GPIO name to change from CONFIG_GPIO_LED_HI to CONFIG_GPIO_LED_0.
Regards,
Ryan
Thanks Ryan.
I tried something similar:
if(DEBUG)
XYZ.addr = 0x1000
else
XYZ.addr = 0x5000
But, getting error:
ReferenceError: DEBUG is not defined
at scriptFunc.....
DEBUG is a predefined symbol.
You've likely defined DEBUG as a pre-defined Compiler symbol, however SysConfig is run before the Compiler builds the project. As the SysConfig environment does not expect pre-defines, you can set a constant value directly in the file instead:
// @cliArgs --board /ti/boards/CC26X2R1_LAUNCHXL --rtos tirtos7
const DEBUG = 0;
/*
* empty.syscfg
*/
var Power = scripting.addModule("/ti/drivers/Power");
/* ======== Kernel Configuration ======== */
system.getScript("kernel_config_release.syscfg.js");
/* ======== GPIO ======== */
var GPIO = scripting.addModule("/ti/drivers/GPIO");
var gpio = GPIO.addInstance();
gpio.$hardware = system.deviceData.board.components.LED0;
if(DEBUG==0) gpio.$name = "CONFIG_GPIO_LED_0";
else gpio.$name = "CONFIG_GPIO_LED_HI";
Regards,
Ryan
Thanks Ryan.
Yes, DEBUG is a predefined compiler symbol.
My intention is to combine two projects (and it's sysconfig files). And the only difference between the two is the symbol DEBUG. And syscfg files have some specific lines for each project, which I thought could be executed separately based on this symbol.
If I set the value as a constant in the file itself, then it defeats the purpose of the if-else running dynamically based on the build configuration.
Would you consider using two different build configurations? That way each can have a different SysConfig file version based on the active build configuration selected.
Regards,
Ryan
Yes, It seems like thats the option I have to choose.
I wanted to combine syscfg also since the difference is only couple of lines.
Thanks
Hi Manoj,
The best solution after speaking with the SysConfig Development Team is to add a scriptArgs flag to Project Properties -> CCS Build -> SysConfig -> Miscellaneous:
--scriptArgs DEBUG
The resultant SysConfig code configuration would appear as such:
// @cliArgs --board /ti/boards/CC26X2R1_LAUNCHXL --rtos tirtos7
console.log(argv);
/*
* empty.syscfg
*/
var Power = scripting.addModule("/ti/drivers/Power");
/* ======== Kernel Configuration ======== */
system.getScript("kernel_config_release.syscfg.js");
/* ======== GPIO ======== */
var GPIO = scripting.addModule("/ti/drivers/GPIO");
var gpio = GPIO.addInstance();
gpio.$hardware = system.deviceData.board.components.LED0;
if(argv[1]==="DEBUG") gpio.$name = "CONFIG_GPIO_LED_0";
else gpio.$name = "CONFIG_GPIO_LED_HI";
Regards,
Ryan