This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI Cloud Agent Multiuser Install on Linux



I'm attempting to install the TI Cloud Agent in a Linux instructional lab (RHEL 7.9)  in which users don't have root access to install the drivers. Is there a way to install TI Cloud Agent for all users or to install the drivers separately, so users can skip that portion of the installation process?

  • Hello,

    If the user does not have root access, then they can still install cloud agent but there will need to be an additional script that is run with root access afterwards. This is a one time step and they should be all set up after this.

    Thanks

    ki