Part Number: CODECOMPOSER
i was trying to install the theme in codestudio - theia but installing not able to set i was given to use two themes one is dark and another is light how do i configure them?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CODECOMPOSER
i was trying to install the theme in codestudio - theia but installing not able to set i was given to use two themes one is dark and another is light how do i configure them?
Hello,
CCS Theia comes with two default themes - Light and Dark. See:
Were you trying to install an use additional themes beyond those two?
Thanks
ki
Which exact themes? and where did you get them from? From the Extensions view?
I installed this theme but I don't see an option to select it either. I'll need to follow up with engineering on if this theme is compatible with Theia IDE.
not only one dark pro any theme is not able to set
could u make it as soon as possible
not only one dark pro any theme is not able to set
Yes I just confirmed with engineering that currently we only support the two default themes (light and dark). It is not possible to add other themes and use them with CCS Theia.
This is something that we can add down the road. But we do not have a specific timetable yet.