Hi,
I am using CCSv5(Version: 5.1.0.07001) under Ubuntu.
I tried to install "the target management terminal" to CCS.
But I could not do it. I had error messages as the following.
Cannot complete the install because of a conflicting dependency.
Software being installed: Target Management Terminal 3.0.2.R31x_v200911051655-7N-FBcBbPtZLuz-SHv_pcfLSKR22 (org.eclipse.tm.terminal.sdk.feature.group 3.0.2.R31x_v200911051655-7N-FBcBbPtZLuz-SHv_pcfLSKR22)
Software currently installed: Shared profile 1.0.0.1314948785666 (SharedProfile_epp.package.cpp 1.0.0.1314948785666)
Only one of the following can be installed at once:
Target Management Terminal Widget 3.1.0.v201106081330-40-7w312217192441 (org.eclipse.tm.terminal.feature.jar 3.1.0.v201106081330-40-7w312217192441)
Target Management Terminal Widget 3.0.0.v200905272300-4--7w311A16383411 (org.eclipse.tm.terminal.feature.jar 3.0.0.v200905272300-4--7w311A16383411)
Target Management Terminal Widget 3.0.1.v200907301400-4-07w311A18412511 (org.eclipse.tm.terminal.feature.jar 3.0.1.v200907301400-4-07w311A18412511)
Target Management Terminal Widget 3.0.2.R31x_v200911051655-4-17S42yaw312113271141 (org.eclipse.tm.terminal.feature.jar 3.0.2.R31x_v200911051655-4-17S42yaw312113271141)
Cannot satisfy dependency:
From: Shared profile 1.0.0.1314948785666 (SharedProfile_epp.package.cpp 1.0.0.1314948785666)
To: org.eclipse.tm.terminal.feature.jar [3.1.0.v201106081330-40-7w312217192441]
Cannot satisfy dependency:
From: Target Management Terminal Widget 3.0.2.R31x_v200911051655-4-17S42yaw312113271141 (org.eclipse.tm.terminal.feature.group 3.0.2.R31x_v200911051655-4-17S42yaw312113271141)
To: org.eclipse.tm.terminal.feature.jar [3.0.2.R31x_v200911051655-4-17S42yaw312113271141]
Cannot satisfy dependency:
From: Target Management Terminal 3.0.2.R31x_v200911051655-7N-FBcBbPtZLuz-SHv_pcfLSKR22 (org.eclipse.tm.terminal.sdk.feature.group 3.0.2.R31x_v200911051655-7N-FBcBbPtZLuz-SHv_pcfLSKR22)
To: org.eclipse.tm.terminal.feature.group [3.0.2.R31x_v200911051655-4-17S42yaw312113271141]
What was wrong? Please advise me.
Best regards,
Michi