Part Number: CODECOMPOSER
Hi experts,
My customer is using CCS 12.6.0.00008 on following setup and facing “Internal Error” when starting CCS.
CCS Version: 12.6.0.00008
CPU:11th Gen Intel(R) Core(TM) i7-1165G7 @ 2.80GHz
RAM:16.0 GB
OS:Windowss 10 Enterprise
Note: installed by using Windows single file (offline) installer
Please see below screenshot for details.

They are using 4 PCs and facing the same issue on all of them..
Please advise me what should I check.
Regards,
Shibata