This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need parameters for silent installation V12.6.0



I am searching for silent install parameters for CCS 12.6.0 unattended installation

in documatiation  for Version 12.6.0 8.1. General — Code Composer Studio 12.6.0 Documentation  / https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_faqs.html#how-can-i-perform-a-silent-or-unattended-installation-of-ccs

is described

8.2.11. How can I perform a silent or unattended installation of CCS?

CCS can be installed from command line interface with several options, including unattended installation. Please refer to the CCS Installer Usage article for more details.

when click on the link " CCS Installer Usage article " > https://software-dl.ti.com/ccs/esd/documents/ccs_installer-cli.html

the article is from old 9.2.0 Version and the Installable Product families are different from Version 12.6.0.

  • Hello,

    the article is from old 9.2.0 Version and the Installable Product families are different from Version 12.6.0.

    Please note that the installer has not changed much since CCS 9.2.x and the documented command should still be relevant for current CCS versions.

    Installable Product families are different from Version 12.6.0.

    Which are the differences you noticed? The list appears pretty accurate and up to date. The only thing I see missing is MSPM0. For that one you can use PF_MSPM0.

    Thanks

    ki