Other Parts Discussed in Thread: BIOSLINUXMCSDK, TMS320C6678
We recently received the C6678 EVM board and the CCS V5 installation SW CD that goes with the package. My job is to take the SW that we run on a C64 and rehost and evaluate it on the C66. My previous experience with CCS is version 2.
From the CD that came with the C66 EVM board, I installed what I thought was the full complement of support and development SW. As directed by the Quick Start Guide card that came with the package, I double clicked on D:\CCS_5.0.3\setup_CCS_5.0.3.00023 (where D is the CD driver of my PC.) After installing the SW, I viewed the welcome video which showed the "Hello world" program being developed and run in CCSV5. I then tried to do the "Hello world" exercise myself to get acquainted with the development environment (my last experience was developing C64 SW with CCS V2.) I encountered the following issues:
1) After configuring the project type as C6000, when I went to compile I got a message saying I didn't have the C6000 Code Generation Tools. I went to the CD and double clicked on D:\CCS_5.0.3\setup_CCS_5.0.3.00023\install_images\cgt\ti_cgt_7.2.1_setupwin32. This enabled me to compile, but shouldn't the global install have provided the tools?
2) In the "Hello world" exercise, when I got to the step where you create the Target Configuration, I saw no options for any C6x processors or the TI simulator. How do I get these into the picture?
Do the above issues imply something went wrong with my installation?
Denise Cammarata