This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: Manually unpacking .pak components from Code Composer .dmg

Part Number: CODECOMPOSER

Hi,

I downloaded the CCS installer .dmg (for 12.5.0), for installation on my mac. I don't have any problems with the installation.

But, since I'm curious, I was looking at the contents of the mounted .dmg, and found the components directory:

$ ls /Volumes/CCS_INSTALLER/components/
ALL-12.5.0.00007-osx.pak DEV_SUPPORT_CC26XX-12.5.0.00007-osx.pak EMU_HERCULES-12.5.0.00007-osx.pak PF_CC2X-12.5.0.00007-osx.pak TARGET_CONTENT_CORE-12.5.0.00007-osx.pak
ARM_CGT_HELP-12.5.0.00007-osx.pak DEV_SUPPORT_CC3220-12.5.0.00007-osx.pak EMU_TI-12.5.0.00007-osx.pak PF_CC3X-12.5.0.00007-osx.pak TIREX-12.5.0.00007-osx.pak
C2000_CGT_HELP-12.5.0.00007-osx.pak DEV_SUPPORT_CC3230-12.5.0.00007-osx.pak INSTALLER-12.5.0.00007-osx.pak PF_HERCULES-12.5.0.00007-osx.pak TIREX4-12.5.0.00007-osx.pak
CCS_DOC-12.5.0.00007-osx.pak DEV_SUPPORT_CC32XX-12.5.0.00007-osx.pak MSP430_BUILD_DEBUG-12.5.0.00007-osx.pak PF_MSP430-12.5.0.00007-osx.pak TIVA_STELLARIS_DRIVERS-12.5.0.00007-osx.pak
CCS_LAUNCHER-12.5.0.00007-osx.pak DEV_SUPPORT_CC32XX_COMMON-12.5.0.00007-osx.pak MSP430_CGT_HELP-12.5.0.00007-osx.pak PF_MSP432-12.5.0.00007-osx.pak TIVA_TM4C-12.5.0.00007-osx.pak
CCS_UTILS-12.5.0.00007-osx.pak DEV_SUPPORT_PGA-12.5.0.00007-osx.pak MSP430_GCC_SUPPORT-12.5.0.00007-osx.pak PF_MSPM0-12.5.0.00007-osx.pak TI_ARM_CLANG-12.5.0.00007-osx.pak
CGT_DEFAULTLIBS_C2800-12.5.0.00007-osx.pak DMED-12.5.0.00007-osx.pak MSP432_BUILD_DEBUG-12.5.0.00007-osx.pak PF_PGA-12.5.0.00007-osx.pak USERGUIDE-12.5.0.00007-osx.pak
CGT_DEFAULTLIBS_MSP430-12.5.0.00007-osx.pak DS-12.5.0.00007-osx.pak MSPM0-12.5.0.00007-osx.pak PF_TM4C-12.5.0.00007-osx.pak core-12.5.0.00007-osx.pak
CGT_DEFAULTLIBS_TMS470-12.5.0.00007-osx.pak DS_FLASH-12.5.0.00007-osx.pak NODEJS-12.5.0.00007-osx.pak SEGGER_J_LINK-12.5.0.00007-osx.pak
CLOUDAGENT-12.5.0.00007-osx.pak EMU_C2000-12.5.0.00007-osx.pak PF_C28-12.5.0.00007-osx.pak SYSCONFIG-12.5.0.00007-osx.pak
DEV_SUPPORT_CC2538-12.5.0.00007-osx.pak EMU_C2000_FLASH-12.5.0.00007-osx.pak PF_CC2538-12.5.0.00007-osx.pak TARGETDB_DEF_PROPS-12.5.0.00007-osx.pak

What kind of files are these '.pak' files? I can't seem to unzip, untar them or anything. How can I unpack them and browse them? It would be interesting to find out. Is there an alternative place from which to download these individual resources?

Where I'm coming from is that I'm keenly interested in continuous integration, DevOps automation and automated workstation setups, so naturally I'm excited by the possibility that there are resources here that I could access in a programmatic way without performing a CCS installation.

Kind regards

Ben  

  • Hi Be,

    What kind of files are these '.pak' files?

    Our installer is based off InstallBuilder. The *.pak are InstallBuilder specific archive files. It is not possible unzip or view the contents in any conventional way. There is no publicly available tool I am aware of that would allow this.

    Thanks

    ki