This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP Project Using CCS v2.21.0.

I have a CCS project targeting a C6711 DSP that I have inherited and need to compile. It was originally setup for CCS v2.21.0 which is not available for download. I have attempted to migrate this project to v3.3.83.20 and 8.3.1 and have had various issues with each. Is there a place I can download v2.21.0?