This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have an input widget (gc-wdiget-input) with id "input_6".
In a Javascript function, how do I get the value of input_6?
For example, I tried this:
var input = GcWidget.querySelector('#input_6').value;
var s = `Input is ${input}`;
alert(s);
which did not work. The string is output as "Input is undefined"
Thanks!