Hi,
I have an EVM5505 with on board VC5505. I am using it with a SpO2 Analog front end. I am trying to make the EVM stand alone using the IIC EEPROM IC (24WC256) on board of the EVM.
These are the steps i follow:
1. Make boot image (.bin) file from SpO2.out using hex55.
2. Burn the .bin file into the programmer.out functionality
I get a message of "Programming Complete"when i burn it to the IIC EEPROM, but the device does not run, after start-up.
I tried the same using the NAND Flash on the EVM and the same .bin file works well and the device functions as a stand-alone.
Is there a problem of using the IIC EEPROM with the SpO2 MDK code ?
Regards
Abhishek