This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5535 eZdsp Quick Start Problem

I was working through the Quick Start "manual" and ran into a problem with section 6 (CCS Configuration Instructions), step 8 (Target->Connect Target).  I get the following error message:

 

C55xx: GEL Output: 

StartUp()

C55xx: Error connecting to the target: (Error -600 @ 0x0) A required dynamic library could not be located. The library isn't on the search path. (Release 5.0.429.0) 

I installed in a different directory than the default (Vista claimed there would be a problem -- I think it was creating subdirectories). I suspect either a path problem or a missing library file.