Other Parts Discussed in Thread: MSP430F5438A
I've seen this problem recurring with CCS v5.1M7 & CGT v3.3.3 when building for MSP430F5438A.
The run-time error check flags valid code as a syntax error and the subsequent build fails--but only if the source file is open in the editor (thus triggering the run-time check).
The code in question is part of Georges Menie's printf-stdarg.c code which is included in the MSP430X distribution of FreeRTOS:
if( *format == 's' ) {
register char *s = va_arg( args, char* );
pc += prints (out, s?s:"(null)", width, pad);
continue;
}
And the error given is: "Symbol 's' could not be resolved".
If I close and re-open the project, then rebuild without opening printf-stdarg.c, the project builds without error. Once the file has been opened, however, the project will not build successfully until closed and re-opened again.
How can I turn off the run time error checking?
Thanks & Regards,
--Mike