Just got a brand new ezdsp5535. Installed CCS that comes on CD, v4.2.4.0033. Installed not on C:\ (it complains), but on another internal HDD F:\ with UAC set to zero-all down. Windows 7 64-bit.
If I connect the USB (after CCS installation), with SD inserted, the USB speaker device comes up and works. Also a composite USB device shows up.
If I remove the SD card, and connect the USB, I got an error in Device Manager with unknown driver TMSC5505 (?). I cannot find any driver for this brick.
In any of two cases above, if I compile a simple program, and use software simulator, it works ok.
When I decide to set up the proper target, namely the "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator" with device EZDSP5535, I always get the "Error initalizing emulator".
List of tries done:
- reboot n->oo times
- changed USB ports
- removed USB drivers
- reinstalled CCS
- checked the registry to remove any residual Spectrum Digital keys
- upgraded (CCS Help->Software Updates) to latest Spectrum Digital drivers
- upgraded (CCS Help->Software Updates) to latest CCS tools (now 4.3.9)
Wonder if I should put this board into the dustbin.
Any help greatly appreciated.