Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TMS320F28377D
Hello,
I encountered those errors when I was debugging or loading projects. I use the TMS320F28377D with XDS100v2 USB Debug Probe, and the project is the example test_application of diagnostic libraries of f2837xd. The operator system is windows7 64x. Testing Connection is successful and the errors only occur when I debug or load projects.
I have reinstalled the CCS for several times and also tried different versions of CCS like CCS7.4, CCS10.4, CCS12.6, but the same errors still occured. I also tried reducing the TCLK frequence but it doesn't work. I tried creating new project instead of importing existing example project, but the errors still occured.
There is no problem when I load the same project into the same board using another computer(windows11) with CCS12.6.
Best Regards,