This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS with Matlab

Hi,

is there any way to exchange data between CCS (version 4 or 5) and Matlab? CCS should use data from real target or simulator (simulator is even better option at this point). I'll give brief example of such application: there is algorithm scripted in matlab and C++ implementation. Input data is generated by matlab and sent to target via CCS. next results are sent back to matlab and compared. 

I'm little bit afraid the only solution is DSS which I've found quite difficult in past. If so, is there any complete example in Java of using DSS?

Thanks in advance

 

regards

MS

  • Hi Michael,

    There is no such support out of the box. A you mentioned, it is possible to use DSS. Some people have already done so on this forum. If you search for "matlab" in the forum, you should find several threads where people have tried to get this going.

    Thanks

    ki