Other Parts Discussed in Thread: DM3730
I followed the instructions in http://processors.wiki.ti.com/index.php/ETB to set up a trace control on the DM3730 board from LogicPD.
I am using the Blackhawk USB 560-M emulator with the 20 pin JTAG cable.
When I set up the Trace Control i.e. Tools->Trace Control, select CSETB and click OK, I get the message
Failed to execute runnable (java,lang.UnsatisfiedLinkError: isSTM)
Unhandled event loop exception
Even if I ignore this and run the code and set up trace jobs, I do get the above message again and I dont see any trace Data recorded.
Please help.