This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5.1.0.08000 does not discover DSP/BIOS install

Guru 15580 points

Gents,

Congrats on the good progress on CCSv5.1!! Keep up the good work.

I have just installed v5.1.0.08000 (yes, I am a glutton for punishment...:). When attempting to build one of my DSP/BIOS projects I get a build error saying that the project was created with a version of DSP/BIOS tools that is not installed. I then installed DSP/BIOS v5_41_07_24 in the same directory as ccs (C:\ti\ccsv5 & C:\ti\bios_5_41_07_24). However, CCS does not auto-discover the DSP/BIOS install, and I cannot figure out how to manually install it. Can you give me some guidance?

Thx,

MikeH